This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40190: More accurate FB pin buck controller

Part Number: TPS40190

Hi Team,

Do we have more accurate FB pin buck controller?

I saw TPS40190 FB pin tolerance is +/- 1%. Do we have +/- 0.5% or lower device?

Vin = 19V Vout = 0.8V Iout=19A

BR,

Roy