Hello team,
I know DCAP 3 control adjusts the switching frequency when the minimum on time restriction is violated to keep the output voltage regulated. My question is: is this recommended? Or should operating close to the minimum on time be avoided?
Specifically, my customer wants to run a 13Vin/.75Vout rail set at 800kHz. My math shows that the max fsw for these conditions is .75/13*1/(85ns) = 680kHz. Is there any issue with setting the switching frequency to 800kHz and having it run actually at ~680kHz while it is limited by the min on time?
It looks like the datasheet has efficiency curves for 800kHz set point with 12Vin/0.6Vout which violates the min on time req so that's why I'm thinking it's okay, but would love to know your thoughts.
Thanks,
Michael