This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for the NMOS design recommendation

Other Parts Discussed in Thread: CSD13202Q2, CSD17577Q3A, CSD17581Q3A

Hi Sir,

 

My customer would like design NMOS power MOS with conditions below.

 

  • The Rdson is better below 5mhom and VDS is 8V~10V.
  • Package is 2*2mm2

 

Would you please provide recommendation for this?

 

 

BR,

SHH

  • Hi Scott,

    Nice to hear from you again. Is this the same application we discussed previously on e2e and over regular email? We have a load switch FET selector tool available at the link below. The lowest rds(on) in 2x2mm SON is the CSD13202Q2 which is 7.5mOhm typical at VGS = 4.5V. In order to get to 5mOhm max, you will have to go to a larger 3x3mm SON package. Some possible devices are:

    • CSD17577Q3A, 4.8mOhm max at VGS = 10V
    • CSD17581Q3A, 4.7mOhm max at VGS = 4.5V