This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: Operation of BQ25606 when D+/D₋ is not used and battery is not connected

Part Number: BQ25606


Dear all,

I would like to ask following questions about BQ25606

1. From the following description in the data sheet, is it correct to recognize that Vsys (system side voltage) is typ.3.68V (min.3.5V) even when the battery is not connected? .

2. Is it correct to recognize that if the D+/D₋ pin is not used, it can be left floating?
(There is no problem with the input current limit value set by RILIM connected to the ILIM pin.)

Best Regards,

Y.Ottey