Other Parts Discussed in Thread: UCC256403
I have a customer working on an LLC (LCC-type for wide Vin) resonant design, and considering the UCC256404. But he has some questions, and your help would be hugely appreciated.
The UCC256404 will be used for a DC input voltage. (Range: 120Vdc ~ 420Vdc)
The UCC256404 was selected vs other variations because the "Bulk Voltage Sense" was lower.
Seems like it will work better with 120Vdc ~ 420Vdc input range....<-- comment from customer
[1]
The HV pins can handle an input voltage range of 120Vdc ~ 420Vdc no problem, yes?
[2]
Is there a way to disable the X-discharge function of the xx404 device?
The datasheet says it works up to 5uF capacitance, but they plan on a much higher capacitance. (The input is DC, not AC)
If there is a higher capacitance, does it just mean it will take longer than IEC60950, IEC60065, IEC62368 specified to discharge the cap?
(Again, they prefer the UCC256404 vs the 403 because of the Bulk Voltage Sense being lower...but if you have any comments on this too...?)
[3]
On the EVM, there are three resistors connected to the HV pin (R26 ~ R28) for about 5kΩ. How do you select what resistance to use here?
https://www.ti.com/tool/UCC25640EVM-020#technicaldocuments
[4]
Section 8.4.2 X-Capacitor Discharge in the DS says you need max 10MΩ parallel resistance for every 100nF. For 330nF, the DS says this is 3MΩ (basically three 10MΩ resistors in parallel), but in the EVM, for 470nF, instead of the 2.5MΩ you would expect, they use 4 series 10MΩ resistors = 40MΩ...is this right?
[5]
How do you disable the burst mode?
Hard to tell from the datasheet...do you just follow Option #7 and connect 2422 ~ 3038Ω between the BW pin and GND?
[6]
In the EVM, it looks like the resonant cap C17 is all that is needed to function, but there is also C1...is C1 needed?
If so, is there any literature, or could you explain, what the function of this is?
I know this is a little long, but again, I really appreciate the help!
Regards,
Darren