This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A84A: for Xilinx RFSoC RF power rails

Part Number: TPS7A84A
Other Parts Discussed in Thread: TPS7A84

Hey

For Xilinx RFSoC Power Rails, Xilinx recommend in there PCB design guide (UG583), to use the Intersil/Renesas ILS80101-A/ ILS80102/ ILS80103/ low noise high PSRR LDOs.

can the TPS7A84A be cross reference to that ?

BR

  • Hi BR,

    The TPS7A84 is a lower noise alternative to the ILS80101-A (I could not find the ILS80102 or ILS80103). Additionally, it is much more accurate as with the Any-Out feature there is no need for feedback resistors to set VOUT so you are looking at a worst-case accuracy if 0.75%.

    I hope this answers your question.