Other Parts Discussed in Thread: BQ25505,
Hi,
what is the difference between the BQ25504 and BQ25505?
Thanks
Fred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frederik,
BQ25505 has integrated/fixed VBATUVLO=2.2V, fixed IC high temperature shutdown and additional gate driver for external FETs used to MUX between the rechargeable secondary battery, connected at VBAT_SEC pin and primary, non-rechargeable battery.
BQ25504 has adjustable VBATUVLO with external resistors and adjustable IC high temperature shutdown.
Regards,
Jeff
Thanks Jeff.
Do I see it right that we recommend the BQ25505 instead of BQ25504 for new designs?
Fred