Hi team.
I'd like to know about the VBUS_UVLO falling.
How much is the VBUS_UVLO falling threshold that determines the PG status?
Sincerely.
Kengo.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kengo,
We do not warranty this parameter in the EC table, but from my observation in the lab I can see a typical value of 3.0V ranging to 3.3V.
I hope this resolves your issue,
Ricardo
The maximum falling threshold I observed was 3.3V. VPOORSRC is described in full detail in section 8.3.3.1 of the datasheet. VPOORSRC is typically 3.7V.
The Power Good Indicator is described in section 8.3.9.1 and there are four conditions that must be met for PG to go low and the LED to indicate.
1. VBUS above VVBUS_UVLOZ: we have discussed that for rising this is a typical value 3.3V as warrantied in the datasheet, for falling I observed a typical falling value of 3.0V but this is not warrantied in the datasheet.
2. VVBUS_OV: rising and falling are described and warrantied in the EC table, please review this.
3. VBUS must be above VPOORSRC (typical: 3.7V) when IPOORSRC (typical: 15mA) is drawn.
4. Input Source Type Detection completed, please review section 8.3.3.2
I hope I helped resolve your questions,
Ricardo