Are there any issues with the LP3985-5.0 starting up into a pre-bias condition where the pre-bias will always be lower than Vin? It will also be lower than the output set point.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are there any issues with the LP3985-5.0 starting up into a pre-bias condition where the pre-bias will always be lower than Vin? It will also be lower than the output set point.
Thanks!
Hi Allen,
The only concern with a pre-biased output is the there is a parasitic diode from VOUT to VIN which means reverse current will flow and charge up VIN. As long as this current is not excessive and the absolute maximum ratings of the device are not violated this regulator will function.
A device like the TPS706 mitigates the reverse current leakage issue.
Does this answer your question?