This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340-Q1: Schematic confirmation with high output capacitance

Part Number: TPS55340-Q1
Other Parts Discussed in Thread: TPS55340

We have a design that requires a high output capacitance and wanted to confirm the TPS55340-Q1 will be able to handle everything. We are looking for a 24V to 36V boost with maximum 2A current output, although the normal current output will be roughly 200mA. We require at least 220uF output capacitor to handle some current surges during operation.

I have used your TPS55340 Boost Calculator Tool and wanted to confirm the circuit. Please let me know if there are any potential issues with the TPS55340 handling this type of operation.