Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24095: TS setting

Part Number: BQ24095
Other Parts Discussed in Thread: BQ24078, BQ24232H

Hi,

Could you let me know Vh and Vc of BQ24095?

Are they 0.278V and 1.23V?

Customer is finding 0~45C, standalone, no JEITA, up to 0.35A charge current, 4.35V regulation device.

I found BQ24078 but it didn't support 0~45C. I couldn't find resistor value for it.

Could you let me know that BQ24095 support these requirements?

Thanks

  • Hi David,

    Yes, for BQ24095 Vhot = 0.278 V  , Vcold = 1.23 V.

    Customer is finding 0~45C, standalone, no JEITA, up to 0.35A charge current, 4.35V regulation device.  BQ24095 meets these requirements. A power-path device that also works here is BQ24232H.

     


    Best,