Hi support team,
It is used with 12V input and 3.3V output.
However, when the load is light (probably a few mA), about 3.6V is output.
Do you know what caused it?
When a load current of about 15mA is applied, it stabilizes at 3.3V.
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi support team,
It is used with 12V input and 3.3V output.
However, when the load is light (probably a few mA), about 3.6V is output.
Do you know what caused it?
When a load current of about 15mA is applied, it stabilizes at 3.3V.
Regards,
Dice-K
Dice,
The output voltage should be slightly higher at light load due to the Power Save Mode operation. 3.6 V seems excessive though. Can you provide waveforms showing Vout and SW for both conditions?
Hi John,
Thank you for your reply.
I attach the waveforms.
“01.” is the state that 3.3V is supplied to IC such as logic IC and ADC.
It is not completely unloaded.
Do you know the cause of 3.6V output?
Best regards,
Dice-K
Hi John,
Removing 100uF of Cout and adding 0.1uF of Cin had no effect.
I saw the waveforms of 3.3V and SW when the power was turned on.
It seems that the voltage has risen since switching stopped halfway.
Do you know what the cause is?
Best regards,
Dice-K
Dice,
In the case where the output goes to 3.6 V, does it always recover after some time?
Hi John,
The cause of 3.6V was found.
The voltage of the IC on the load side was sneaking into Vout.
I apologize for the inconvenience.
Best regards,
Dice-K