Hi Qian,
Are there any known issues with DCM when using the LM5119 in interleaved mode (single output)?
I am seeing multiple LM5119 failures at > 40V input voltage / no load on the output with DCM, but in CCM this problem seems to disappear.
In both cases, the output is well regulated, the switching waveforms look good, and there is minimal overshoot on the switching node. Just with DCM the LM5119 has spurious failures, and this does not seem to happen with CCM.
The no load power dissipation is obviously higher with CCM - can I use the EN2 input to disable channel 2 when the output current is low? Or is this dangerous in interleaved mode?
Kind regards,
Andrew