This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27762: Issue with LM27762 (wrong input and outpu voltage)

Part Number: LM27762

Hello,

I'm having issues with the LM27762 on two different PCB. 

On one of them, i have the right negative output but the positive output is not regulated. Indeed, the positive output, whic should be 3.3V, is equal to the input voltage which is 5V.

On the other one, the input voltage should be 5V but it doesn't even reach the 5V. The input capacitor doesn't fully charge, it's a really weird behavior...

Can you help me with that? I tried everything, including changing the IC but i'm running out of ideas.

Here are the schematic and the layout :