Hi Sir,
customer design TPS61042. from spec, the max Vfb is 260mV.
however, customer measure the Vfb is 0.263~0.266mV.
Is there any side effect for this?
Vin: 5.09V
RS;13Ohm
BR,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
customer design TPS61042. from spec, the max Vfb is 260mV.
however, customer measure the Vfb is 0.263~0.266mV.
Is there any side effect for this?
Hi SHH,
260mV is a max. value under the typical application conditions. Since customer's application is different from the datasheet, a little difference is acceptable for internal reference voltage. In a word, customer don't need be worry about this.
BR,
Robin