Hi Support Team,
According to the BQ25792 datasheet
Ship Mode when SDRV_CTRL[1:0] = 10. The ship FET and the internal BATFET are both off. The I2C is still enabled. The charger can be woken up by setting SDRV_CTRL[1:0] back to 00, or pulling the QON pin low, or an adapter plug-in. This mode is only for the battery only condition
#1 What I don't understand is; if Ship FET is OFF, the battery is completely disconnected, how does the device remain powered up and accept I2C commands?
Input Current Limit
In the application circuit, V(ILIM_HIZ) = 2.2V, i.e. 5v x100k/(127k+100k)
V(ILIM_HIZ) = 1V + 800mΩ × IINDPM, in which IINDPM = 1.5A. However, the design parameters table 67 IINDPM register is set to 12Ch for 3A.
#2 My understanding is that, the input current limit is set by lower setting of ILIM_HIZ pin and the IINDPM register. In this case, IINDPM would be 1.5A and not 3A.
Best,
AJ