Other Parts Discussed in Thread: LM25066
Hi,
I'm using LM25066IAPSQ/NOPB in my new design.
My application needs: 12V Hot swap, insert delay, max 25A current sensing (over and short), UVLO/OVLO, etc,
I added all the relevant components like: CL=25mv, CB=1.8, Rsense=0.001ohm (for 25A), relevant resistors for UVLO/OVLO, Ctimer=22nF and all the rest following you Typical Application Circuit recommendation (attached below my circuit)
My question is: Do I need SW configuration initializations via the SMBus or HW setup is sufficient?
Regards,
Menachem