Hi Guys
The flyback uses UCC28610 and the output voltage is 12V. In the test, under the condition of 170V to 400VDC input, the number of ZCDs is 2 at full load.
problem:
1. Why is the 170V to 400VDC input, full load (continue to increase the load, the chip is in the restart state), the number of ZCD is 2, why does not appear ZCD=1? Datasheet show: at least 1. So what will affect the number of ZCD? The following waveform (Picture 1) is 400VDC input voltage Load=4A, Mosfet's VDS. In the measured waveform, is the time for the free-wheeling (inside the red circle) 2.4 us? Is it related to the Twait (ZCD) time in the datasheet?
Datasheet, Page 7
Picture 1 Vin=400VDS, Load=4A, Signal 2 VDS
2. Observe the waveform of the VDS above (Picture 1, Load=4A). The MOSFET does not turn on Mosfet at the bottom of the resonance. The load is relatively small (Load=3A), when ZCD is equal to 5 (Picture 2), the MOSFET is close to the bottom when it is turned on.
In the case of a relatively large load (Picture 1, Load=4A), the MOSFET has not turned on Mosfet at the bottom. Is it the cause of UCC28610? I tested the waveform at 170VDC and full load at 250VDC, the MOSFET also did not turn on Mosfet at the bottom of the resonance.
Is it necessary to add the capacitor described in the Datasheet to adjust the LC resonance phase to the same phase as the ZCD current? What does the specific opening time here have to do with?
Picture 2 Vin=400VDS, Load=3A, Signal 2 VDS
3. Page27 in the datasheet. What is the meaning of tWAIT in the circle?
Does this mean that the IDRV output, or the time between Ton and the first detected ZCD, must be at least 7.5us in time difference?
Thanks
-Vincent