Other Parts Discussed in Thread: LM317
Hi All
Hope all are fine
BQ2002T how can we set chargine current or it has inbuilt fast charging means what is the charging rate ?
Either the charging current is adjustible or fixed
My specifications
Input : 5V 500mA USB
Battery: 2 cells NImh 1.2V /800 mAh
Charging current expected : 0.5C
Termination Style: Change in temperature /Cahnge in voltage
Can you guys give me a better circuit or recommend an IC which meets above specs in TI