Tool/software: WEBENCH® Design Tools
I am using tps61088 regulator, so it is not compatible with the date sheet and Webdesign. In the case of WEBDESIGN provided by TI, the design input of TPS61088 is 6V to 8.4V (2 cells of lithium ion battery), and the output is 12V to 3A or more. It was not designed when more than 30W of power was designed. When contacting TI support, WEBDESIGN is said to be designed considering limits not written in the datasheet. However, the TPS61088 EVM board was used to load up to 58W from the DC loader. What is the exact limit Watt of tps61088??