Other Parts Discussed in Thread: LMZM33606
Hello,
I've noticed that with deafould PCB configuration (directly of the shelf) the converter behaves in strange way:
When DC supply is applied first, then 5A load everything is ok,
but when I've got the load applied first (1Ohm resistor at 5V) then I connect 20Vdc input the output goes low to about 3V and 5A.
Is it normal LMZM33606 behaviour?
Regards,
Adam