This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH05050W: PTH05050W module internal schematic

Part Number: PTH05050W
Other Parts Discussed in Thread: TPSM82480

Hi team,

My customer is using PTH05050WAH to convert 5V input to 2.5V output. But sometimes the PTH05050 output becomes to 0V.

To find the root cause of the issue, we want to do some test on the PHT05050 module. But this module integrates some discrete component and we don't have the module schematic so we don't know what is the function of each discrete component and how they are connected. So can you help provide the PTH05050 module internal schematic so we can test which part is malfunction. Thanks.

Best regards,

Wayne

  • Hi Wayne,

    These devices are not meant for debugging of their internal nodes.

    Maybe you can share some details of the specific case via email?  When does the output go to 0V?  Is this during development or in the field?  Does the output ever recover?  How many devices show this behavior and how many have been tested?

    Finally, we have newer 6A modules such as the TPSM82480.