Other Parts Discussed in Thread: TPS62090
Hi Team,
1. The datasheet shows that FREQ has internal pull-down, so when I change to 2.8MHz, I only need to drop the pull-up resistor NC?
2. In customer‘s application, they change from 5V to 4V. However, when the input of TPS62090-Q1 change from the main supply 5V to the backup battery 3.7V, what is the output voltage of TPS62090? 0V?
2. Our project uses TPS62090QRGTRQ1 5V to 4V when it works normally; When the front-end 5V voltage is switched to battery-powered, that is, the input voltage becomes 3.7V, the output voltage will be directly equal to 3.7V or another value.