Other Parts Discussed in Thread: BQ40Z60
Hello, everyone,
I wonder if the BTP function works correctly? Every time I connect the power supply on the evaluation board, the BTP-INT bit is set, even if the RSOC has 10% or higher.
Are there any other parameters that influence BTP?
my configuration:
Init discharge set = 150mAh
init charge set = 175mAh
pack capacity = 6000mAh
NR = 1 & EMSHUT_EN = 0 & PCHGBTP = 1 & BTP_EN = 1
my configuration on the board:
The BTP interrupt function is enabled by removing the shunt from the J7 jumper and installing a shunt from SYSPRES to ALERT on the J2 jumper.
Kind regards and thanks
Riccardo