Part Number: BQ76940
Hi, TI
Q1. Besides AFE input power droop, Is that any other case that can cause Xready triggered?
Q2. If It is a WatchDog issue, How can I identify it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ76940
Hi, TI
Q1. Besides AFE input power droop, Is that any other case that can cause Xready triggered?
Q2. If It is a WatchDog issue, How can I identify it?
Hi Shang,
XREADY will trigger when 5 of the 8 communications between cell groups internal to the part are corrupt in a 1 second interval. The part considers the reported result unreliable in this condition and turns off FET outputs. Some common causes:
1. Missing power on upper groups such as droop as you indicate causing reset of the group
2. Broken or missing power connection
3. Shorted CAPn capacitor
4. TSn having trapped voltage at boot due to missing pull down
5. Pull down of TSn below its reference (abs max violation)
6. Large noise on power pins
7. Some customers have reported XREADY in high field strength environments, it is not know if the entry is through the power pins or TSn to a remote thermistor or other. Filtering and shielding are the expected solutions.