This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCP020515D: DCP020515D Max Channel Output Current

Part Number: DCP020515D

Hello,

the DCP020515D datasheet states a max device output current of 133mA (IOUT1 + IOUT2).
Is there an additional restriction of keeping the output current at max 66mA per channel?
Or would it be fine to use 100mA on one channel (+ or -) and 33mA on the other (- or +)?

Thanks,