This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5176: LM5176

Part Number: LM5176

Tool/software: WEBENCH® Design Tools

Hello,

I using LM5176 for 15V 25A power. I found the output voltage touch OVP voltage(17.3V VFB 0.882V) during no load condition. If I add 20mA resistor load to output the out output voltage back 15V.  

How can we slove this problem?

Vin 12V,

Vo set 15V, measure 17.3V during no load.

Lei