Hi Expert,
I am not able to find the duty cycle range, what's the max and min output voltage with input voltage 5V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
I am not able to find the duty cycle range, what's the max and min output voltage with input voltage 5V?
Hi team,
I got update from customer. This will be used under these two application.
1. VDDQ: 1.2V/ 12.14A
2. VCCSA: 1.05V/ 11.1A
Is that OK to support with 5V input voltage?
Oliver,
I believe no webench available for this part, but you can try pispice model for simulation at Ti.com
Yuchang