This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61043: Operation mode

Part Number: TPS61043
Other Parts Discussed in Thread: TPS61042,

Hi

In the datasheet shows the Bust (boost?) mode operation waveform. How do we use this operation at TPS61043 (or TPS61042)?

We'd like to constant LED current.


- Connect to TP1410: typ.1.5V (changing by feed back circuit)
- 4 LED: Not white LED, typ.1.6V Vf / 1 LED
- CTRL: connect to 3.0V_REG
- LED current: about 3 - 40 mA (typ. about 15mA)

- R2 = 58kohm (43k+15kohm)

- R1 = 5.1kohm

- RS = 6.8ohm

Best regards,

KoT