Other Parts Discussed in Thread: BQ24232, BQ25616, BQ25896
Dear Sir or Madam,
we are working on an architecture study for battery powered embedded system. Battery will be LiPo with 1800mAh.
I have studied available chargers and found the BQ24250 which supports an I2C control interface. And I found the BQ24232 which seems to be suited as well, but does not feature an I2C control interface.
What is the advantage of the I2C control interface? Is it recommended if the system can support I2C (as in our case; we have a Linux System) to make use of that? Or could the system as well be configured to use an autonomous charger for the sake of simplicity and less effort on the SW dev side?
Could you please explain? Or share a document explaining the advantages of a charger with control interface vs one without?
Many thanks in advance & Kind Regards,
thomas