Hi,
I will have the following questions:
1. The charger only looks at the voltages on VBAT_OV every 64ms that means the VRDIV node is monitored to samples and holds the VSTOR voltage.In addition to power consumption, does this situation affect my dynamic adjustment though the resistor to set the output to dynamic output?If it is possible in theory, can my output also can be dynamically changed every 64ms?
2. According to data manual 7.4.3 shows One way to avoid cold start is to attach a partially charged storage element.If VBAT_SEC connection a depleted energy storage components such as super capacitor and energy collector provided is not enough, lead to chip cannot exit cold start, but in BQ25505 VBAT_PRI we have prepared a primary non-rechargeable batteries, we can through the primary battery to charge the VSTOR above 1.8 V firstly to make the circuit out of cold start, so that the booster work?I think the principle should be the same with attach a partially charged storage element, please talk about your opinion, thank you very much.
Regards,