Other Parts Discussed in Thread: BQSTUDIO
Hi,
Let me discuss charging current monitoring using the IBAT pin.
Customer is not able to detect charging current using IBAT.
However, the measurement of the discharge current has been successful.
They measure by connecting a digital multimeter to the IBAT pin.
Could you give me some advice as to why the charging current cannot be monitored?
And Please advise about the register setting and connection method necessary for correct IBAT charge current monitoring.
Register settings related to the IBAT is the following.
ADD:0x12H Charge Option 0
Bit[12] = 0b IDPM AUTO DISABLE
Bit[1] = 1b IDPM Enable
ADD:0x3BH Charge Option 1
Bit[11] = 1b IBAT Enable
ADD:0x38H Charge Option 2
Bit[6] = 1b IBAT OUTPUT SELECT
ADD:0x15H Max Charge Voltage Register
0x2EE0H
ADD:0x14H Charge Current Register
0x0400H
Best regards
Yusuke