Other Parts Discussed in Thread: TPS62561, TPS62560, TPS62590
Sorry if someone else already covered this, but I did see it.
The data sheet shows a low res capture of a single transition on the input, but I am seeing problems with over all noise rejection. My input has noise in the 200mV range at 20 to 30KH, and if the regulator is loaded, this noise passes right through. Also high freq (above 5Mhz) noise seems to also pass right through. I am using a 10uf X5R cap on the input side of the regulator and a 22uF x5R cap on the output (both MLCC) (3.3uF inductor). I know my supply could be cleaner, and that is one way I can address this problem, but it seems that the TPS62561 should be able to provide a stable output with ripple voltage less than 50mV without problems. (These regulators feed digital circuits, which work fine with noise below 50mv, but at 150mv they start failing.)
I know I likely did something stupid in the design, but any feed back would be appreciated.
Thanks.