Hi,
Assume
Vbus1 = 12V and Vbus2 = 5V
Case: When EN pin of Vbus1 controller is pulled low
The load will still see Vbus1 voltage (12V) due to body diode conduction. Is this right?
If yes, what is the exact functionality of the EN pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Assume
Vbus1 = 12V and Vbus2 = 5V
Case: When EN pin of Vbus1 controller is pulled low
The load will still see Vbus1 voltage (12V) due to body diode conduction. Is this right?
If yes, what is the exact functionality of the EN pin?
HI
When ORing two power supplies of same voltage rail for example, 12V, both can be ON at the same time and supply load current together.
But for if you need to turn off one rail for any reason, then using EN, will turn off the MOSFET and prevent that rail from supplying power to the load.
Though body diode conducts small current, it needs output voltage (OR-ed) to go below one diode drop to conduct.
Let us know if this answers your question.
Regards,
Kari.