Other Parts Discussed in Thread: TPS61090
I am designing a device that requires a 5V DC input source and want to provide a 3.7V li-ion battery for backup only. I want to use the BQ24075 for power path management and battery charging, but need a stable 5V output also when running off the battery. Is the design choice to combine it with the TPS61090 boost stage a common/recommended combination with the BQ24075? The load will never draw more than 2A peak, and mostly <1A.