This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2813-0-Q1: Boost converter solution

Part Number: UCC2813-0-Q1
Other Parts Discussed in Thread: UCC28C40-Q1, , UCC28951-Q1

Dears,

I'm looking for the best solutions of automotive application's high power boost converter. But It is not easy to find that solutions. Could you recommend it for me? The requirements are as follows.

Input voltage : 240V(dc) to 420V(dc), Output voltage : 420V(dc), Po=3.5kW

I'm considering the PWM controllers of UCC2813-0-Q1 and UCC28C40-Q1. Please share the best solutions and related document with me.

Regards,

Jeffrey