Hi Team,
Just want to check if Cin and Cout can be decreased to 1x10uf respectively when max Iout is 330mA. Thanks.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Just want to check if Cin and Cout can be decreased to 1x10uf respectively when max Iout is 330mA. Thanks.
BRs
Given
Hi Given,
Nice to see you again. It's okay to have a 10uF input cap but for the output. To confirm whether TPS7A84A could work with a 10uF output cap with the reduced maximum current, we would need to rerun some simulations. Let's have a quick sync call during your morning time and I will take this support via direct email since this is against datasheet recommendation.
Regards,
Jason Song
Using less than 47uF is against datasheet recommendation,