This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A84A: Cout at low current

Part Number: TPS7A84A

Hi Team, 

Just want to check if Cin and Cout can be decreased to 1x10uf  respectively when max Iout is 330mA.  Thanks. 

BRs

Given 

  • Hi Given, 

    Nice to see you again. It's okay to have a 10uF input cap but for the output. To confirm whether TPS7A84A could work with a 10uF output cap with the reduced maximum current, we would need to rerun some simulations. Let's have a quick sync call during your morning time and I will take this support via direct email since this is against datasheet recommendation. 

    Regards, 
    Jason Song

    Using less than 47uF is against datasheet recommendation,