This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5108: Negative Voltage Transient on HS Pin

Part Number: LM5108
Other Parts Discussed in Thread: UCC27282

Hello,

We are evaluating the LM5108 and had a question on the Negative Voltage Transient capability of the HS Pin.

The abs max voltage range on HS pin is -5 to 105V.  Is the -5V a DC voltage value?  Is there lower voltage transient specification?

Thank you, Keith