This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A90: LDO Feedback loop resistor selection

Part Number: TPS7A90

Hi,

I am using TPS7A9001 LDO in one of the design.

Input is 4.2V and output is designed for 3.4V

As per datasheet (Page 18) for 3V3 the recommended Feedback resistor values is  3.57K and 1.15K.

Since, it is connecting to internal error amplifier and error amplifier is voltage driven, i am planning to use 100K and 30K so that, the Feedback current will be further reduced.

Will this cause any issues for the performance of the IC for long term?

Please suggest, what is the recommended range of feedback pin current?

Can we use 100K and 30K in our design?

or do we need to follow as per datasheet recommendation values?

Regards,

Harish.