I would like to use REF3012 with VIN=1.8V.
I found an answer "It is ok if it is slightly lower than 1.8V. The only time 1.8V comes into effect is if the device is sourcing its max current." in the thread 'REF3012: Minimum voltage spec'.
The error in the supply voltage is unavoidable, so I would like to know how low VIN REF3012 can work correctly. The output current is expected to be less than 1mA. At this time, how low VIN is possible? Also, is there any document that correlates the output current and VIN?
thanks,