Part Number: TPS60400-Q1
Other Parts Discussed in Thread: TPS60400, TPS60140, REG710-33, SN74AHCT1G08
We would like to make a 3.3V-5V power supply by boosting from the LDO output power supply of about 2.5V, 40mA. I would like to use Charge Pump Power IC such as TPS60400, not DCDC converter for boosting because the supply current is limitted by 40mA(voltage is 2.5V). The output of this boost power supply needs to drive only one CMOS buffer IC with a power consumption of 10mA. On the other hand, I have heard that Charge Pump boost power IC couldn't drive CMOS IC. So, I concerned about whether I can use Charge Pump Power IC such as TPS60400 for CMOS Buffer IC.
Can I apply Charge Pump Power IC such as TPS60400 to drive CMOS IC(ex. TC7SET08FU) ? Is the driving ability enough?
If there are any other concerns, I would be happy if you could give me some advice. Thank you.