This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
My customer used this device in their system, and the condition is Vin=5V, Vout=3.3V, Iout=500mA. When they test this device's surface temperature with thermocouple under 75°C high ambient temperature, they found that this surface temperature is up to 108°C. The max junction temperature is 125°C in the datasheet. If 108+ψJT*(5-3.3)*0.5<125, it is ok. But if the result >125, this chip maybe damaged. But now I can't find the value of ψJT in the datasheet, so I am not sure whether 108°C is too high for this device.
Thanks & Best Regards,
Sherry