Part Number: TPS62067-Q1
Other Parts Discussed in Thread: TPS62067
Hi All,
In the datasheet of TPS62067, there is one sentence to define the feedback resistor value.
To minimize the current through the feedback divider network, R2 must be within the range of 120 kΩ to 360 kΩ. The sum of R1 and R2 must not exceed approximately 1 MΩ in order to keep the network robust against noise.
But some customer has limitation to use resistor no larger than 100Kohm, so if customer can accept large current through the feedback resistor, which the minimum feedback resistor value can be used for TPS62067?
Best Regards
Charles Zhang