Other Parts Discussed in Thread: TIDA-00779,
Dear expert,
In the
TI DESIGNS TIDA-00779 REVB Bom, description for c14 is
CAP, CERM, 8.2 μF, 25 V, +/- 10%, X5R, 0603
In schematic C14 is also 8.2uF.
But the part no. written in the BOM is
0603ZD475KAT2A
Which is 4.7uF capacitor.
Which value is the correct one 4.7u or 8.2uF?
Regards
Barry Ng