Hello, we are experiencing a lot of 'swollen' batteries from the field lately due to field personnel using the wrong adapter supplying VDD. When this occurs, the 29200 allows VDD across one battery (2 18650 in series) which obviously is way beyond the max rating. Obviously, the way to fix it is for them to use the correct power adapter however... hasn't happened yet!
Just wondering if there's a easy solution to sense the over-voltage condition on either battery and disable the 29200? We have a very limited board space.
Thanks
Dan Ross - AST