This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5012: LP5012 as replacement for LP55231

Part Number: LP5012
Other Parts Discussed in Thread: LP55231,

Hi, E2E,

One of our projects used the LP55231 as the main LED driver of the system, for the next revision we would like to replace it with a device capable of driving 12 channels and configured to operate with common anode configuration.

The LP5012 seems to be a good solution. Will the LP5012 work properly with this LED and a single +3.3V supply (for both VCC and VLED)?. Do you have another recommendation apart from LP5012?.

Thanks in advance for your help.

Best Regards,

  -Diego Melendez

  • Hi, Diego Melendez,

    LP5012 is a good choice which can meet your needs. The constant-current with high precision is up to 25.5mA Maximum per channel In full range and 35.5mA Maximum per channel when VCC>=3.3V. it is properly with the target LED.

    Best Regards

    Monet Xu