Other Parts Discussed in Thread: CSD83325L, BQ2980
I’m curious about the FET choice because our over-current thresholds are going to be very low (250-350mA). I originally picked a small FET (CSD83325L) to start and with 20mΩ Rds,on we end up with a 5mV or so voltage threshold (outside the trimmable range)
Would you suggest picking a FET with higher resistance or could we do something like add an 0201 sized resistor in series with the FET to increase the effective Rds,on?
Also, how long does it take to get a custom factory programmed part?
Will we be better off sizing Rds,on (perhaps with the series R) to match a catalog device?
Thanks,
Nick