Hi,
I want to built a wireless charger for a small battery (100mAh - 300mAh). I came across the BQ51050B, but I read it is not suitable for such small batteries. The suggested alternative is the TIDA-00318 solution, but it has ICs that are very difficult to solder by hand. Just to check, would a combination of the BQ51013B and BQ2404x be suitable for a small battery?
Also, is it possible to nicely shut down wireless power if charging is finished with this combination? The ~CHG and EN1 don't seem nicely compatible, or am I missing something? (If ~CHG starts low, I think it might work, but I'm not sure if it does).
Best regards,
Samot