Other Parts Discussed in Thread: BOOST-PSEMTHR-007, , TPS2373-4EVM-758, TPS23881, USB2ANY
Hi Teams,
Customer is evaluating PoE with TPS2373-4EVM-758, TPS23881EVM-008, BOOST-PSEMTHR-007.
They use autonomous mode by shorting a bottom of J5 in EVM (=4 pair 90W). After that, they connect J19 and J21 of the PSEMTHR and PD side of 4-pair, and tried to increase a load current. Both reach 5.3A (30W) as the highest, so were not able to reach the bt opreration.
They also done evaluation at only PD device. It reached 14A so it works well.
Do you think there are any issue on PSE device?